AXIS#.WS.DISTMIN

Description

This parameter sets the minimum movement that is required for commutation finding. If this value is too small, then the commutation finding might fail if too little current is used. The larger this value, the more movement is needed in order to avoid F5500: "Wake and Shake - Insufficient movement".

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Actual position units

Range

0 to 90 deg

Default Value

1 deg

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.DISTMIN

5013h

0fh

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6702

1

6702 (0x1a2e)

AXIS1.WS.DISTMIN

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.DISTMIN

6702

Signed32

Read/Write

Position